earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Poradnik

Poradnik


Produkty: AS-B, Enterprise Central, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
Funkcje: Trendy
Wersja produktu: 3.2, 3.3, 2022
2020-10-15

Viewing a Trend Log in a Temporary Trend Log List

You open a trend log in a temporary trend log list to view the recorded values in a list. When you close the temporary trend log list, the list is not saved.

Pokaż więcej
action_close

​To display a trend log without creating a new trend log list or trend chart, the trend log can be displayed in a temporary list or chart.

 
action_zoom_plus_stroke Trend log displayed in a temporary trend log list and temporary trend chart
Rysunek: Trend log displayed in a temporary trend log list and temporary trend chart
Uwaga

You have to manually refresh the trend log list.

To view a trend log in a temporary trend log list
  1. In WorkStation, in the System Tree pane, select the folder or EcoStruxure BMS server where the trend log is located.

  2. Select the trend log you want to open as a temporary trend log list.

  3. On the Actions menu, point to View and then click In Trend Log List .

(In FM: TaskClosing) The trend log list is displayed in the work area under a generic name.

  • Temporary Trend Log Lists
  • Saving a Temporary Trend Log List
  • Temporary Trend Charts
  • Viewing a Trend Log in a Temporary Trend Chart