You configure the Archive settings and schedule on the Enterprise Server to automate the archiving process.
In WorkStation, on theTools menu, click Control Panel.
On the Control Panel toolbar, select the Enterprise Server.
Click Archiving.
Under Archive Settings, click Enabled.
Select the events that you want to include in the archive:
Alarm Events: Select to include high priority or off-normal events (providing the alarms are pre-configured and active on the system).
User Events: Select to include user-initiated events, such as value overrides or configuration changes.
System Events: Select to include device-initiated events, such as time stamps.
Click the Add extended trend logs button
In the Include column, select the extended trend logs and click OK.
Under Archive Schedule, click Schedule to create recurring exception and calendar events.
In the Output Type box, select the format you want to use for the archive:
CSV: This output generates data separated by a delimiter.
XML: This output generates data using a standard internet protocol.
In the Path box, type the path to an existing archive directory where you want to store the archive files.
Click Validate to confirm that the path is valid on the system.
A check mark
When finished, click the Save button