earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-P-3, AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Alarms
Product version: 7.0, 7.1
10/30/2025

Create Alarm Wizard – Presentation Page

Use the Presentation page to configure the presentation settings of the alarm.

 
action_zoom_plus_stroke Presentation page
Figure: Presentation page

Table: Presentation Page

Component

Description

Above upper limit message

​Type the message to display when the variable exceeds the upper limit of the alarm.

Below lower limit message

​Type the message to display when the variable falls below the lower limit.

Alarm message

Type the message to display when the alarm is in Alarm state.

For more information, see Alarm Messages .

Reset message

​Type the message to display when the alarm is reset.

For more information, see Alarm Messages .

Category

​Enter the category the alarm belongs to.

For more information, see Categories .

Category 2

Enter the second category the alarm belongs to.

For more information, see Categories .

Prefix for alarm source name

Add a substitution code or type a prefix that is added to the beginning of the source name property of an alarm record.

For more information, see Substitution Codes for Notifications .

Above upper limit priority

​Enter the priority level of the alarm when the variable exceeds the upper limit.

For more information, see Priority .

Below lower limit priority

​Enter the priority level of the alarm when the variable falls below the lower limit.

For more information, see Priority .

Alarm priority

Enter the priority level of the alarm.

For more information, see Priority .

Reset priority

​Enter the priority level of the alarm when it is reset.

For more information, see Priority .

Same priority

Select to set all priorities to the same value.

For more information, see Priority .

Auto hide

Select to automatically hide the alarm in the Alarms pane or Alarm View.

For more information, see Alarm Decoration .

Flashing alert

Select to make the alarm row flash in the Alarms pane and Alarm Views when the alarm is triggered.

For more information, see Alarm Decoration .

Audible alert

Select to make the alert audible when the alarm is triggered.

For more information, see Alarm Decoration .

Custom audio

Enter the path to the custom audio file you to play when the alarm is triggered.

For more information, see Custom Audible Alarm Alerts.

Disable state-change logging

Select to prevent an alarm state change from creating an event.

For more information, see Alarm State-change Logging .

  • Alarm Functions
  • Create Alarm Wizard – User Action Page
  • Create Alarm Wizard – Attachment Page
  • Create Object Wizard – Naming the Object Page
  • Substitution Codes for Notifications
  • Alarm Messages
  • Categories
  • Priority
  • Alarm Decoration
  • Custom Audible Alarm Alerts
  • Alarm State-change Logging