Image Widget Dialog Box
Use the
Image Widget
dialog box to add or replace an image.
action_zoom_plus_stroke
Figure:
Image widget dialog box
Table: Image Widget Dialog Box
Component
|
Description
|
Image
|
Browse to the image you want to display in the image widget.
|
Image Stretch
|
Select how you want the image to be displayed in the image widget.
Select
Cover
to fit the image into the image widget without any resizing.
Select
Fit
to adjust the image to fit in the image widget. The image is resized without losing its proportions.
Select
Fill
to adjust the image to fit in the image widget. The image is resized and lose its proportions.
|
How Dashboards Work
Dashboard Widgets
Image Widget
Widget Dialog Box – Layout Tab