earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Sustainability
7/2/2025

Resetting a Meter Object

You reset a meter object, for example, after a testing. After the reset the meter object restart calculations and logging.

To reset a meter object
  • Do one of the following:

    • In WorkStation, right-click the meter object, point to Meter management then click Reset consumption value and clear trend log . In the Reset dialog, click Yes .

    • In WebStation, right-click the meter object, then click Reset consumption value and clear trend log . In the Reset meter dialog, click Reset meter .