Use the Basic tab to view and update basic properties of the clean contact output.
Property |
Description |
Index |
Displays the index, which is a unique number set by the fire detection system. |
IO function |
Displays the IO function. For more information, see MCU, IOC and OCA clean contact and monitored relay output functions . |
Contact description |
Displays the contact description, as defined in the configuration. |