earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: FDP Server
Functionalities: Engineering
7/4/2025

Zone test mode

Warning Warning

REDUCED RESPONSE TO FIRE

  • Take all necessary precautions, for example, posting guards in relevant positions, before you activate test mode for a zone.

  • Comply with any applicable legislation, regulations, standards and/or guidelines regarding actions to be taken when parts of the fire detection system are unresponsive.

  • Deactivate zone test mode again at the earliest opportunity.

Failure to follow these instructions can result in death, serious injury, or equipment damage.

When zones are in test mode, detectors in these zones do not trigger fire alarms in the fire detection panel.

Note:

You can activate zone test mode only if there are no faults in the zone

  • Zone Properties – Basic Tab