earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: FDP Server
Functionalities: Engineering
6/10/2026

ALC, SLC, ELC and LC output function and output function 2

In the address table, double-click the cell in the Output function or Output function 2 column to see a menu of available output functions.

Table: Output functions

Output function

Description

Not in use

N/A

Fire alarm device output

Activated if there is a fire alarm

Fire alarm device output, non-silenceable

Activated if there is a fire alarm. Cannot be silenced with the 'Silence' button. Use this option for, for example, beacons.

Fire alarm device level 1 silenceable output

Activated if there is a fire alarm. Can be silenced with the 'Silence' button on access level 1.

Fault warning device output

Activated if there is a fault

Voice evacuation activated output

Activated if there is a fire alarm

Voice evacuation test output

Activated if a fire alarm device control test or a voice evacuation test output control test is activated

Fire alarm output

Activated if there is a fire alarm

Prealarm output

Activated if there is a pre-alarm

Fault warning output

Activated if there is a fault

Main supply fault output

Activated when a fault in the mains supply is detected

Maintenance warning output

Activated if there is a maintenance alert

General reset output

Activated for 30 seconds when a reset sequence (of any alarm type) starts

Fire door output

Activated if any of the conditions set in the FIRE DOOR CONTROL view is fulfilled

Extinguisher output

Activated if there is a fire alarm

Disablement output

Activated if anything is disabled in this panel or its visible panels

Zone disabled output

Activated if the zone that the module belongs to is disabled

Access level output

Activated if the key is turned to the operating position

Technical alarm output

Activated if there is a technical alarm

Internal logic output

Activated by the built-in control logic

External logic output

Activated by an external control logic

Delayed fire alarm output

Activated when the panel has delayed fire alarms

Fire alarm router activated LED output

Activated if the Fire routing activated LED is lit

Delayed alarm enabled output

Activated if delayed alarms are enabled

Fire router disabled output

Activated if the fire alarm router is disabled

Fault router disabled output

Activated when the fault warning router is disabled