earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: ​License Administrator, ​License Server
Functionalities: License Management
2/11/2025

Order Information Request

All licenses bought from a Schneider Electric vendor are delivered in an entitlement. The entitlements specify the products and features you are allowed to use.

For more information on how to order, contact your local EcoStruxure BMS vendor.

Entitlements

The entitlement ID is the designation that represents the license purchased by the customer. This ID is included in the entitlement that is sent by email when an order is approved.

The email with the entitlement also contains an HTML-file, the Entitlement Certificate File. This file is important when you add and set up the entitlement in Device Administrator.

Licenses for EcoStruxure Building Operation software and for field servers are delivered in entitlements.

  • License products for EcoStruxure Building Operation software are managed by License Administrator.

  • License products for field servers are managed by Device Administrator.

  • Mixed entitlements that contain licenses managed by Device Administrator and licenses managed by License Administrator. Device Administrator and Licenses Administrator has a built-in filter that only allows the correct administrator to manage the licenses. For example, when a mixed entitlement is added to Device Administrator, only the licenses in the mixed entitlement that is managed by Device Administrator is visible and can be used using Device Administrator.

You can add one or many entitlements to Device Administrator or License Administrator.

 
action_zoom_plus_stroke An example of an Entitlement.
Figure: An example of an Entitlement.

You can of course, at any time, buy a new entitlement with new products that you add to your site.

Product

A product may contain one or many features. All products have an activation ID that is used then the product is activated.

Order number/Seat count/Number of licenses

The product may contain one or many licenses for a specific feature.

Example

You have a site with five field servers. You want all field servers to use SNMP notification and you want all the users of the field servers to be able to create personal dashboards.

 
action_zoom_plus_stroke An example of an Entitlement for field servers.
Figure: An example of an Entitlement for field servers.
 
action_zoom_plus_stroke Example of an Entitlement for EcoStruxure Building Operation software
Figure: Example of an Entitlement for EcoStruxure Building Operation software

EcoStruxure Building Operation Software License Order Request

The order request process involves License Activation Server and License Server.

 
action_zoom_plus_stroke Workflow when requesting order information for EcoStruxure Building Operation software
Figure: Workflow when requesting order information for EcoStruxure Building Operation software

Table: Request Order Information for EcoStruxure Building Operation software

Number

Description

1

The Entitlement ID , which contains the licenses to activate, is entered into the License Administrator.

2

The License Administrator sends the entitlement ID to the License Activation Server.

3

The License Activation Server sends the order information to the License Administrator.

For more information, see EcoStruxure Building Operation Software Licensing Workflow .

Field Server Licensing Order Request and Entitlement Setup

The order request process for field server licensing involves Device Administrator, License Activation Server, and the field server.

 
action_zoom_plus_stroke Work flow when requesting order information for field servers
Figure: Work flow when requesting order information for field servers

Table: Request Order Information for Field Servers

Number

Description

1

The Entitlement ID , which contains the licenses to activate, is entered into Device Administrator.

2

Device Administrator sends the entitlement ID to License Activation Server.

3

License Activation Server sends the order information to Device Administrator.

  • Licensing Overview
  • EcoStruxure Building Operation Software Licensing Workflow