Our site will be unavailable from October 29-30 due to scheduled maintenance.
Thank you for your patience.
You configure Windows Firewall for Connect Agent to ensure that the system and crash information is available on Connect storage server.
On the Windows toolbar, select Start and then click Control Panel .
Click System and Security and then click Check firewall status .
Click Advanced settings and then click Outbound Rules .
Click New Rule .
Select Program and click Next .
Enter the SE.SBO.S2ConnectESAgent.exe program path. (For example, C:\Program Files (x86)\Schneider Electric EcoStruxure\Building Operation x.y\S2ConnectAgent\bin\SE.SBO.S2ConnectESAgent.exe). Click Next .
Select Allow the connection and click Next .
Select the profiles and click Next .
In the Name box, type the name for the rule.
Click Finish .