earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Device Administrator, FDP Server
Functionalities: Engineering, License Management
10/30/2025

Show Licenses View Toolbar

Use the Show Licenses view toolbar to manage licenses.

Table: Show Licenses View Toolbar

Button

Description

Add Server

Click to add a field server to the list. For more information, see Automation Server Connection .

Assign Licenses

Click to assign licenses on the selected field server. For more information, see Assign and Activate Licenses .

Activate

Click to activate licenses on the selected field servers. For more information, see Assign and Activate Licenses .

Return

Click to return licenses on the selected field servers. For more information, see Return Licenses on Field Servers .

Reclaim

Click to reclaim licenses on the selected field servers. For more information, see Reclaim Licenses .

Refresh License Status

Click to refresh the license status on the selected field servers.

Other

Click to open the Other menu. For more information, see Other Menu .

Current state

Select to view the current status of the activated licenses.

Edited state

Select to view the sum of assigned and activated licenses.

Show licenses

Select to show the Show licenses view toolbar.

  • Assign Licenses View
  • Automation Server Connection
  • Field Server Licensing on Field Servers not Connected to Internet Workflow
  • Assign and Activate Licenses
  • Return Licenses on Field Servers
  • License Settings Dialog Box