earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Device Administrator, FDP Server
Functionalities: License Management
11/15/2025

Software and Features that Require Licenses

A number of software and features need licenses.

EcoStruxure Building Operation

Refer to the document Part Number Summary and Hardware Software Matrix for software and features that need licenses, available on Schneider Electric Extranet.

Information regarding licenses can also be found on the specification sheets:

For more information, see WorkStation .

For more information, see WebStation .

For more information, see Enterprise Central .

For more information, see Enterprise Server .

For more information, see Compliance Pack .

EcoStruxure Fire Operation

Information on which licenses that are available for EcoStruxure Fire Operation are found in the specifications:

For more information, see WorkStation .

For more information, see WebStation .

For more information, see FDP Server .

For more information, see Enterprise Central .

For more information, see Enterprise Server .

  • Licensing Overview
  • EcoStruxure Building Operation Software Licensing Overview
  • Field Server Licensing Overview