earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Device Administrator, FDP Server
Functionalities: Engineering, License Management
3/6/2025

Add Entitlement from File

Use the Add Entitlement from file dialog box to add the entitlement.

 
action_zoom_plus_stroke Add Entitlement from file dialog box
Figure: Add Entitlement from file dialog box

Table: Add Entitlement from File Dialog Box

Command

Description

Browse

Browse to the entitlement file.

  • Field Server Licensing on Field Servers Connected to Internet Workflow
  • Field Server Licensing on Field Servers not Connected to Internet Workflow
  • Restarting Field Servers from Device Administrator
  • Add Entitlement from ID
  • Checking Entitlement Dialog Box
  • Contacting License Activation Server Dialog Box