earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: FDP Server
Functionalities: Engineering
6/2/2025

MCU and IOC clean contact input functions

Day mode is intended to be changed a few times a day. When day mode has been enabled or disabled, you cannot immediately toggle it again.

Warning Warning

UNEXPECTED DAY MODE STATUS

  • Wait at least one minute before you toggle day mode again after you have enabled or disabled it.

  • Verify that the panel has the correct day mode status.

Failure to follow these instructions can result in death, serious injury, or equipment damage.

Toggling day mode generates numerous event messages. Consequently the fire detection panel rejects any requests to toggle day mode for a minute after it has been changed. The aim is to avoid overloading communication lines in the fire detection system.

Clean contact input functions

Description

Not in use

The input is not in use and has no effect

Customer LED 1 activation input

Activates the 1 LED on the panel

Customer LED 2 activation input

Activates the 2 LED on the panel

Day mode and delayed alarm enable input

Sets this panel and its visible panels in day mode and enables delayed alarms

Day mode enable input

Activates day mode for this panel and its visible panels

Delayed alarm enable input

Enables delayed alarms for this panel and its visible panels

Delayed alarm reset input

Resets delayed alarms for this panel and its visible panels

Evacuation activation input

Activates all fire alarm devices of this panel and its visible panels

External logic input

Provides a signal to an external control logic

Extinguisher activated input

Activates the ‘Extinguisher input activated’ indication

Extinguisher fault warning input

Activates a fault that indicates ‘Extinguisher fault’

Fault warning in fault warning router input

Activates a fault that indicates ‘Fault router fault’

Fault warning in fire alarm router input

Activates a fault that indicates ‘Fire router fault’

Fault warning input

Activates a fault

Fire alarm device mute input

Temporarily mutes (disables) fire alarm devices of this panel and its visible panels when a Voice Evacuation message is announced

General reset input

Resets alarms

If there are alarms with different priorities (fire alarm, pre-alarm, fault and maintenance), only alarms with the highest priority are reset

General silence input

Silences alarms

If there are alarms with different priorities (fire alarm, pre-alarm, fault and maintenance), only alarms with the highest priority are silenced

Internal logic input

Provides a signal to the built-in control logic

Local day mode and delayed alarm enable input

Sets this panel in day mode and enables delayed alarms

Local day mode enable input

Activates day mode for this panel

Local delayed alarm enable input

Enables delayed alarms for this panel

Local evacuation activation input

Activates all fire alarm devices of this panel

Local fire alarm device mute input

Temporarily mutes (disables) fire alarm devices of this panel when a Voice Evacuation message is announced

Maintenance warning input

Activates a maintenance alert

Silent technical alarm input

Activates a technical alarm, excluding the buzzer

Smoke ventilation activated input

Activates the Smoke vents activated LED on the panel

Start delay T2 for delayed alarm input

Starts timer T2 for delayed alarms for this panel and its visible panels

Technical alarm input

Activates a technical alarm, including the buzzer

Voice evacuation fault warning input

Activates a fault that indicates 'Voice evac. fault input activated'