earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: FDP Server
Functionalities: Engineering
6/2/2025

SLC device types

In the address table, double-click the cell in the Type column to see a menu of the available device types. Some of the menu items have sub-menus.

Type menu

Type sub-menu

0 - Not in use

1 - Ionisation smoke detector

Ionisation smoke detector, 200 series

2 - Optical smoke detector

0 - Optical smoke detector, Advanced series

1 - Optical smoke detector, 200 series

3 - Static thermal detector

0 - Static thermal detector, Advanced series

1 - Static thermal detector, 200 series

G - Rate-of-rise thermal detector

0 - Rate-of-rise thermal detector, Advanced series

1 - Rate-of-rise thermal detector, 200 series

H - High temperature thermal detector

0 - High temperature thermal detector, Advanced series

1 - High temperature thermal detector, 200 series

9 - Laser detector, LZR-1

Laser detector, 200 series

A - Laser detector, 7251

Laser detector, 200 series

B - Multi-criteria detector

0 - Multi-criteria detector, Advanced series

1 - Multi-criteria detector, 200 series

D - Three-criteria detector

0 - Three-criteria detector, Advanced series

1 - Three-criteria detector, 200 series

E - Four-criteria detector

0 - Four-criteria detector, Advanced series

1 - Four-criteria detector, 200 series

F - Beam detector

0 - Beam detector, Advanced series

1 - Beam detector, 200 series

Y - Beam detector with test filter

I - Manual call point, indoor

Advanced series

J - Manual call point, outdoor

Advanced series

5 - Single input module

0 - Single input module, Advanced series

1 - Single input module, 200 series

Z - Single input module, mini

Advanced series

L - Dual input module

Advanced series

M - Dual input, single output module

Advanced series

6 - Single output module

0 - Single output module, Advanced series

1 - Single output module, 200 series

N - Single output module, 240V

Advanced series

7 - Conventional zone module

0 - Conventional zone module, Advanced series

1 - Conventional zone module, 200 series

X - Conventional zone module, CZR Advanced series

S - Wall mounted sounder

Advanced series

T - Wall mounted sounder strobe

Advanced series

U - Wall mounted strobe

Advanced series

V - Detector base sounder

Advanced series

W - Detector base sounder strobe

Advanced series

C - Any type (virtual)*

8 - Any type**

*) No physical device needs to be installed. This can be set in alarm condition only through an alarm test or through the INFO protocol.

**) A physical device must be installed.