earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: FDP Server
Functionalities: Engineering
6/2/2025

MCU, IOC and OCA clean contact and monitored relay output functions

Clean contact output functions

Description

Not in use

The output is not in use

Access level output

Activated when the panel is in access level 2

Delayed alarm enabled output

Activated when delayed alarms are enabled

Delayed fire alarm output

Activated when the panel has delayed fire alarms

Delayed fire alarm T2 output

Activated when timer T2 for delayed alarms is running

Disablement output

Activated if anything is disabled in this panel or its visible panels

External logic output

Activated by an external control logic

Extinguisher output

Activated if there is a fire alarm

Fault router disabled output

Activated when the fault warning router is disabled

Fault warning device output

Activated if there is a fault

Fault warning output

Activated if there is a fault

Fault warning router equipment output

Activated if there is a fault

Fire alarm device level 1 silenceable output

Activated if there is a fire alarm. Can be silenced with the 'Silence' button on access level 1.

Fire alarm device output

Activated if there is a fire alarm

Fire alarm device output, non-silenceable

Activated if there is a fire alarm. Cannot be silenced with the 'Silence' button. Use this option for, for example, beacons

Fire alarm output

Activated if there is a fire alarm

Fire alarm router activated LED output

Activated when the Fire routing activated LED on the panel is lit

Fire alarm router equipment output

Activated if there is a fire alarm

Fire door output

Activated when any of the selected conditions for the fire door control are active

Fire router disabled output

Activated when the fire alarm router is disabled

General reset output

Activated for 30 seconds when a reset sequence (of any alarm type) starts

Internal logic output

Activated by the built-in control logic

Mains supply fault output

Activated when a fault in the mains supply is detected

Maintenance warning output

Activated if there is a maintenance alert

Prealarm output

Activated if there is a pre-alarm

Technical alarm output

Activated if there is a technical alarm

Voice evacuation activated output

Activated if there is a fire alarm

Voice evacuation test output

Activated if a fire alarm device control test or a voice evacuation test output control test is activated

The selectable functions for monitored relay output functions are the same as for clean contact outputs.