earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: FDP Server
Functionalities: Engineering
6/2/2025

ALC device types

In the address table, double-click the cell in the Type column to see a menu of available device types. Some of the menu items have sub-menus.

Select the Intellia variant for Essentia devices.

Type menu

Type sub-menu

0 - Not in use

1 - Ionisation smoke detector

0 - Ionisation smoke detector, Intellia

1 - Ionisation smoke detector, Discovery

2 - Ionisation smoke detector, XP95

3 - Ionisation smoke detector, S90

1 - Optical smoke detector

0 - Optical smoke detector, Intellia

1 - Optical smoke detector, Discovery

2 - Optical smoke detector, XP95

3 - Optical smoke detector, S90

4 - Optical wireless smoke detector, XP95

3 - Thermal detector

0 - Thermal detector, Intellia

1 - Thermal detector, Discovery

2 - Thermal detector, XP95

3 - Thermal detector, S90

4 - Thermal wireless detector, XP95

4 - High thermal detector

0 - High thermal detector, XP95

1 - High thermal wireless detector, Discovery

5 - Multi-criteria detector

0 - Multi-criteria detector, Intellia

1 - Multi-criteria detector, Discovery

2 - Multi-criteria detector, XP95

3 - Multi-criteria wireless detector, XP95

6 - Carbon monoxide detector

0 - Carbon monoxide detector, Intellia

1 - Carbon monoxide detector, Discovery

P - Carbon monoxide thermal detector

0 - Carbon monoxide thermal detector, Intellia

1 - Carbon monoxide thermal detector, Discovery

7 - Beam detector

8 - Flame detector

A - Conventional zone module

Wireless loop interface

B - Manual call point

0 - Manual call point, Intellia

1 - Manual call point, Discovery

2 - Manual call point, XP95

3 - Manual call point, S90

4 - Manual wireless call point, XP95

D - Switch monitor module

C - Switch monitor module with interrupt

J - Single input, single output module

0 - Single input, single output module, XP95

1 - Single input, single output wireless module, XP95

L - Addressable sounder

0 - Addressable sounder, XP95

1 - Addressable wireless sounder, XP95

M - Sounder controller module

N - Beacon

R - Sounder beacon

0 - Sounder beacon, Intellia

1 - Sounder beacon, Discovery

9 - Any type (virtual)*

O - Any type**

*) No physical device needs to be installed. This device type can be set in alarm condition only through an alarm test or through the INFO protocol.

**) A physical device must be installed.