In the address table, double-click the cell in the Output function or Output function 2 column to see a menu of available output functions.
Output function |
Description |
Not in use |
N/A |
Fire alarm device output |
Activated if there is a fire alarm |
Fire alarm device output, non-silenceable |
Activated if there is a fire alarm. Cannot be silenced with the 'Silence' button. Use this option for, for example, beacons. |
Fire alarm device level 1 silenceable output |
Activated if there is a fire alarm. Can be silenced with the 'Silence' button on access level 1. |
Fault warning device output |
Activated if there is a fault |
Voice evacuation activated output |
Activated if there is a fire alarm |
Voice evacuation test output |
Activated if a fire alarm device control test or a voice evacuation test output control test is activated |
Fire alarm output |
Activated if there is a fire alarm |
Prealarm output |
Activated if there is a pre-alarm |
Fault warning output |
Activated if there is a fault |
Main supply fault output |
Activated when a fault in the mains supply is detected |
Maintenance warning output |
Activated if there is a maintenance alert |
General reset output |
Activated for 30 seconds when a reset sequence (of any alarm type) starts |
Fire door output |
Activated if any of the conditions set in the FIRE DOOR CONTROL view is fulfilled |
Extinguisher output |
Activated if there is a fire alarm |
Disablement output |
Activated if anything is disabled in this panel or its visible panels |
Zone disabled output |
Activated if the zone that the module belongs to is disabled |
Access level output |
Activated if the key is turned to the operating position |
Technical alarm output |
Activated if there is a technical alarm |
Internal logic output |
Activated by the built-in control logic |
External logic output |
Activated by an external control logic |
Delayed fire alarm output |
Activated when the panel has delayed fire alarms |
Fire alarm router activated LED output |
Activated if the Fire routing activated LED is lit |
Delayed alarm enabled output |
Activated if delayed alarms are enabled |
Fire router disabled output |
Activated if the fire alarm router is disabled |
Fault router disabled output |
Activated when the fault warning router is disabled |