earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: FDP Server
Functionalities: Engineering
6/2/2025

ELC device types

In the address table, double-click the cell in the Type column to see a menu of the available device types.

Type menu

Not in use

Smoke detector

Heat detector

Multi-criteria detector

Manual call point

4 inputs module

2 inputs, 2 outputs module

2 inputs, 2 monitored outputs module

4 outputs module

Potential output for sounder

Relay output module, 240V

Conventional zone module

Base sounder in standard base

Base sounder beacon in standard base

Base sounder in red/white VAD base

Base with sounder

Base with sounder beacon

Wall mounted sounder

Wall mounted sounder beacon

Any type (virtual)*

Any type**

*) No physical device needs to be installed. This can be set in alarm condition only through an alarm test or through the INFO protocol.

**) A physical device must be installed.