Day mode is intended to be changed a few times a day. When day mode has been enabled or disabled, you cannot immediately toggle it again.
Toggling day mode generates numerous event messages. Consequently the fire detection panel rejects any requests to toggle day mode for a minute after it has been changed. The aim is to avoid overloading communication lines in the fire detection system.
In the address table, double-click the cell in the Input function column to see a menu of the available input functions.
Input function |
Description |
Conventional zone input |
Fire alarm |
Beam detector input |
Fire alarm |
Input function |
Description |
Wireless expander input |
Transfers communication between the panel and wireless devices |
Input function |
Description |
Not in use |
None |
Conventional line input |
Fire alarm |
Customer LED 1 activation input |
Lights up the ‘Customer LED 1’ indicator |
Customer LED 2 activation input |
Lights up the ‘Customer LED 2’ indicator |
Day mode enable input |
Sets this panel and its visible panels in day mode |
Day mode and delayed alarm enable input |
Sets this panel and its visible panels in day mode and enables delayed alarms |
Delayed alarm enable input |
Enables delayed alarms for this panel and its visible panels |
Delayed alarm zonal reset input |
Resets delayed alarms in the same zone as the monitor module |
Delayed alarm zonal silence input |
Silences delayed alarms in the same zone as the monitor module |
Evacuation activation input |
Activates all alarm devices of this panel and its visible panels |
External logic input |
Provides a signal to an external control logic |
Extinguisher activated input |
Lights up the ‘Extinguisher Activated’ indicator |
Extinguisher fault warning input |
Activates a fault with the ‘Extinguisher fault’ indication |
Fault warning input |
Activates a fault |
Fire alarm device mute input |
Temporarily mutes (disables) the fire alarm devices of this panel and its visible panels when a Voice Evacuation message is announced |
Fire alarm input |
Fire alarm |
General reset input |
Resets the highest priority alarms |
General silence input |
Silences the highest priority alarms |
Internal logic input |
Provides a signal to the built-in control logic |
Local day mode enable input |
Sets this panel in day mode |
Local day mode and delayed alarm enable input |
Sets this panel in day mode and enables delayed alarms |
Local delayed alarm enable input |
Enables delayed alarms for this panel |
Local evacuation activation input |
Activates all alarm devices of this panel |
Local fire alarm device mute input |
Temporarily mutes (disables) fire alarm devices of this panel when a Voice Evacuation message is announced |
Maintenance warning input |
Maintenance alert |
Manual call point |
Fire alarm |
Prealarm input |
Pre-alarm |
Silent technical alarm input |
Technical alarm, excluding the buzzer |
Smoke ventilation activated input |
Activates the Smoke vents activated LED on the panel |
Technical alarm input |
Technical alarm |
Voice evacuation fault warning input |
Activates a fault with the ‘Voice evac. fault input activated’ indication |
Zone disablement input |
Disables the zone to which the module is configured |