earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: User Management
10/30/2025

Type Permissions View

Use the Type permissions view to grant user accounts or user account groups extended access to a specific type.

For more information, see Creating Type Permissions Templates .

 
action_zoom_plus_stroke Type permissions view
Figure: Type permissions view

Table: Type Permissions View

Component

Description

Relative to

Click

 
action_zoom_plus_stroke
to select an instance of the type you want your permission to be relative to.

Type name

Displays the name of your type.

 
action_zoom_plus_stroke

Add

Click to select the object that you want to add to the permission path.

 
action_zoom_plus_stroke

Delete

Click to remove an object that you have added to the permission path.

Relative object

Displays an object or objects added to the permission path.

Read

Select to permit viewing and listing path content.

Write

Select to permit an administrator to change configurations except for bindings, programs, and graphics.

Create

Select to permit creating new objects on the path.

Delete

Select to permit deleting objects under the path. Delete permissions are required on a folder to delete its contents.

Edit

Select to permit editing objects on the path.

Force

Select to permit forcing values on the path.

Command

Select to permit the execution of commands on the path. Command permissions can override this permission for specific commands.

Properties

Click to configure properties.

  • Creating Type Permissions Templates
  • Software Permissions
  • Software Permissions Rules Management
  • Relative Path Permissions
  • Editing Relative Path Permissions Templates
  • Relative Path Permissions Rules