earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: WorkStation, WebStation
Functionalities: Engineering
2/18/2026

Fire Detection Systems

arrow1_rotationFire Detection System Commands arrow1_rotationAccess Levels arrow1_rotationAlarms and States

The main purposes of a fire detection system are to save lives and to minimize damage to buildings and other properties in case of a fire. A fire detection system detects actual fire, risks of fire, and other fire-related events.

Depending on what the system detects, it activates the right type of alarm devices and sends alarms to, for example, the fire brigade and different users. The system also notifies users about other types of alarms and alerts.

A fire detection system consists of components and objects such as fire detection panels, fire controls, loops, loop devices, and zones.

Fire Detection System Commands

You alter state and behavior of the fire detection system and objects in it by executing commands in EcoStruxure Fire Operation.

For more information, see Fire Detection System Commands .

Access Levels

The access level in the fire detection system is set in the panel with EcoStruxure Fire Operation server capabilities.

For more information, see Access levels .

Alarms and States

In a fire detection system, there are different types of alarms, faults, maintenance alerts, tests, and disablements. Various causes generate these alarms and changes in device states.

For more information, see Alarms and states .

  • Fire Detection System Objects
  • Fire Detection System Commands
  • Access levels
  • Alarms and states
  • Fire Detection System Properties – Basic Tab