earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: WorkStation, WebStation
Functionalities: Engineering
2/18/2026

Loop Devices

Loop devices provide functionality for fire detection, smoke detection, input, output, and other necessary features.

Loop devices are installed, configured, and added to a loop in the fire detection system. Examples of loop devices are smoke detectors, multicritera detectors, and I/O modules.

About Loop Controllers

A loop controller is an expansion board in the FDP that allows one or several loops to be created in the configuration.

For more information, see About loop controllers .

ALC, SLC, ELC, and LC input functions

Examples of ALC, SLC, ELC and LC input functions are Day mode enable input, Manual call point, and Zone disablement input.

For more information, see ALC, SLC, ELC and LC input functions .

ALC, SLC, ELC, and LC output function and output function 2

Among ALC, SLC, ELC, and LC output functions and output functions 2 are Fire alarm output, Disablement output, and External logic output.

For more information, see ALC, SLC, ELC and LC output function and output function 2 .

Loop Device Commands

The commands on a loop device are used to enable/disable the device, update values, and perform tests.

For more information, see Loop Device Commands .

Alarms and States

In a fire detection system, there are different types of alarms, faults, maintenance alerts, tests, and disablements. Various causes generate these alarms and changes in device states.

For more information, see Alarms and states .

Requests

In an EcoStruxure Fire Operation setup, requests are used with schedules, Function Blocks, and Script Programs to automatically change state and behaviour of objects such as FDPs, loops, and zones.

For more information, see Requests .

Loop Device Output Test Mode

A loop device has an output test mode that you activate to perform tests on the device.

For more information, see Loop Device Output Test Mode .

  • Fire Detection System Objects
  • ALC, SLC, ELC and LC input functions
  • ALC, SLC, ELC and LC output function and output function 2
  • Loop Device Commands
  • Alarms and states
  • Requests
  • Loop Device Output Test Mode
  • Loop Device ALC Properties – Basic Tab
  • Loop Device CLC Properties – Basic Tab
  • Loop Device ELC Properties – Basic Tab
  • Loop Device SLC Properties – Basic Tab