earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: WorkStation, WebStation
Functionalities: Engineering
1/9/2026

Power Outputs

Besides other functions and features, expansion boards have power outputs. The purpose of a power output is to provide other components with current.

In some cases, for example when a short circuit in a power output occurs, a fault alarm is generated, pointing to the power output.

  • Fire Detection System Objects
  • Expansion Boards
  • Power Output Properties – Basic Tab