earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WorkStation
Functionalities: Basic Functionality
12/17/2024

Viewing a Schedule

You view a schedule using Basic Schedule Editor.

Show More
action_close

The Basic view of the Schedule Editor serves as a workspace to plan and design a schedule. You use this editor to create, manage, and display weekly scheduled events and exception events.

You can also display the client time zone and the server time zone in the Basic view. This is convenient if your EcoStruxure BMS server is located in a time zone that is different from the time zone where you are configuring the schedule. For more information, see Time Zones .

The following figure displays the schedule of the lights within the building. The weekly events are in green and the exception event in blue. The values of the events are also displayed. Monday, November 12 is an exception event so it does not follow the same scheduled events as the rest of the week. The lights are off all day. For the rest of the week, the lights turn on at 07:00 and turn off at 18:00.

 
action_zoom_plus_stroke Basic view of the Schedule Editor
Figure: Basic view of the Schedule Editor

To view a schedule
  • In WorkStation, click on the schedule.

The schedule is displayed in Basic Schedule Editor.

  • How Schedules Work in Fire Operation
  • Basic View of the Schedule Editor