90 Topic(s)
Use the Web Server Certificate dialog box – basic tab to connect to the Enrollment over Secure Transport server and to add Certificate Signing Request (CSR) information.
You configure the global certificate settings so that the EcoStruxure Building Operation servers can communicate with the PKI server using EST.
You configure the communication with the Enrollment over Secure Transport server to request and receive digital certificates.
You disable MD5 hash when you want the EcoStruxure BMS servers to use only strong algorithms for encryption.
You add a device to the whitelist so that it can communicate with the field server.
You can choose which certificate you want to be active.
Use the Add File Extension dialog box to add a file extension to the Permitted File Extensions list.
You activate a certificate so it is in effect.
You add a security banner to your system to notify the user that the user is entering a secure system.