22 Topic(s)
Use the Consumption SignatureWidget dialog box to configure and edit a consumption signature.
A consumption signature chart is a bar chart where you can see expected and actual consumption for a certain period. You can choose if you want to see the alarm limits or not.
The consumption signature object is used to calculate, analyze, and graphically present expected energy consumption.
The consumption signature object is used to calculate, analyze, and graphically present expected energy consumption.
Use the Consumption Signature PlotWidget dialog box to configure and edit a consumption signature plot widget.
Use the Meter Processor– Outputs tab to view the output from the meter processor.
Use the Meter Graph View to display a graphical presentation of the relations between meter objects and meter processors.
You initiate a meter replacement when you want to replace the physical meter that is monitored by the meter object.
Use the Contributions View to display the contributions.
The consumption signature object is used to calculate, analyze, and graphically present expected energy consumption.