179 Topic(s)
Use the Summary tab to edit the basic settings for a user account. For example, you can enable or disable the user account, or change the password for the account.
Use the Type permissions view to grant user accounts or user account groups extended access to a specific type.
You open diagnostics in WebStation to check the health of your system.
You change the password for the local administrator (admin) accounts on the EcoStruxure BMS servers to prevent unauthorized access.
All user account information is stored centrally in the EcoStruxure Building Operation user database, which contains information about software permissions, user account memberships, workspaces, and domains.
As a WorkStation administrator, you can change passwords, track user activities, validate accounts, and set up user and user and user group accounts.
Use the Workspace configuration page to add, edit, and remove workspace components.
Use the Pane configuration page to determine the layout of the component you are adding to the workspace.
Use the Workspace properties to configure the properties of a workspace.
Software permissions limit the paths, objects, and commands that are available in a workspace. For example, a user with No Access permissions for a particular path cannot see any of the path objects displayed in the System Tree pane. A user with Read permissions for a path can see the path objects but cannot issue any commands because the objects are not made available.