1171 Topic(s)
The EcoStruxure Building Operation software gives you a number of functions to monitor and manage your facilities.
An alarm compares the value from a monitored variable with the conditions of the alarm. Different types of alarms handle different types of variables and different forms of evaluation.
Listed below are the System Alarms with IDs that begin with the letters E-L.
Click to get information on the Edit Connection and Add Server dialog boxes in Device Administrator.
EcoStruxure Building Operation software has a number of features that helps you increase the security in your system.
Dynamic XLSX reports and templates combine to enhance flexibility when creating XLSX reports for object data. The dynamicity comes from the ability to configure templates for one or several object types without binding the templates to specific reports or objects. Once you have the templates for the object types you need, making a report is no more difficult than to create a dynamic XLSX report object, add the objects you need a report on and map them to the corresponding template based on their type. Another option is to create the report ad hoc from the context menu by right-clicking on any object in your system.
Use the Basic tab to configure and view the General Information properties.
These hardening guidelines applies to the EcoStruxure Building Operation software products and the EcoStruxure BMS server products.