earth_america
user_standard Log on
earth_america

Enterprise Server

Refine your search
arrow2_down
Refine your search
Ok
Ok
Ok

1251 Topic(s)

Concept

The EcoStruxure Building Operation software supports the major communication protocols in building automation and security management.

Concept

The EcoStruxure Building Operation software gives you a number of functions to monitor and manage your facilities.

Concept

​The change of value trend log records the variable each time the difference between the current value and the last log value exceeds the delta. Use the change of value trend log to, for example, record a variable that has an unequal oscillation.

Concept

An alarm compares the value from a monitored variable with the conditions of the alarm. Different types of alarms handle different types of variables and different forms of evaluation.

Concept

Listed below are the System Alarms with IDs that begin with the letters E-L.

Concept

Click to get information on the Edit Connection and Add Server dialog boxes in Device Administrator.

Concept

EcoStruxure Building Operation software has a number of features that helps you increase the security in your system.

Concept

Dynamic XLSX reports and templates combine to enhance flexibility when creating XLSX reports for object data. The dynamicity comes from the ability to configure templates for one or several object types without binding the templates to specific reports or objects. Once you have the templates for the object types you need, making a report is no more difficult than to create a dynamic XLSX report object, add the objects you need a report on and map them to the corresponding template based on their type. Another option is to create the report ad hoc from the context menu by right-clicking on any object in your system.

User Interface

Use the Basic tab to configure and view the General Information properties.

Specifications