1267 Topic(s)
Use the Building Operation WorkStation window to log on to WorkStation.
You use theDisplay Names and IP Addresses of Servers drop-down list box to add, edit and delete the display names of the server addresses. You also use it to export, import and delete lists of the display names and IP addresses of servers.
You edit a backup rule on an EcoStruxure BMS server to change the type of data that you want to back up. You can also set up this backup rule to follow a shadow schedule that references a lead schedule managed on another EcoStruxure BMS server.
You create an out of reference range alarm to trigger an alarm when a variable, such as a temperature, differs from a reference value.
You create an out of range alarm to trigger an alarm when a variable, such as a temperature, is not within its specified range.
You create an interval trend log to record a value of a variable at specified and regularly occurring increments of time.
You create an extended trend log to store log records for a longer period of time and free up memory in the field server.
You create a change of state alarm to trigger an alarm when a variable, such as a switch, is either true or false.
You back up multiple EcoStruxure BMS servers manually to copy and store data that is frequently updated.
All system events, as well as information and circumstances, are recorded in the Event log. These event records can be viewed in the Events pane or in an Event View.