15 Topic(s)
These hardening guidelines applies to the EcoStruxure Building Operation software products and the EcoStruxure BMS server products.
You view logged server events in the Enterprise Server or Enterprise Central system log to troubleshoot server problems that are traced to the Enterprise Server or Enterprise Central.
The Software Administrator installs with the Enterprise Server and Enterprise Central installation package. You use the Software Administrator to start and stop the server service and configure the ports of the Enterprise Server and Enterprise Central.
You start the server manually in case you previously have stopped it.
Use the Enterprise Server viewto start and stop the Enterprise Server service and configure the ports of the Enterprise Server.
You stop the Enterprise Server to configure the port settings or to repair, upgrade, or reinstall the Enterprise Server.
Before upgrading the system, it is strongly recommended that you archive the historical data and back up the EcoStruxure BMS servers to preserve the current data and configurations.
You start Enterprise Central manually if it has been stopped.
You start Software Administrator to be able to configure the port settings of the Enterprise Server or Enterprise Central.