earth_america
user_standard Log on
earth_america

WebStation

Refine your search
arrow2_down
Refine your search
Ok
Ok
Ok

374 Topic(s)

How to

You sort on alarms and events to get a better overview in the Alarms View or Events View.

How to

You select fields in the Alarm view or Event view to display information regarding alarms and events.

Concept

There are several sets of icons for fire graphics. The icons that are used in your fire graphics depend on the selection of icon set in Fire Expert Graphics manager.

Concept

The set of Swedish icons is used to display Swedish icons in fire graphics.

Concept

The set of Italian icons is used to display Italian icons in fire graphics.

Concept

The set of Finnish icons is used to display Finnish icons in fire graphics.

Concept

The set of default icons are used in fire graphics when no other set is selected in Fire Expert Graphics manager.

Concept

When you force a value, you override all input from the system. For example, if a schedule is set to enable a device at 09:00, but you want to enable it at 08:00, you can force the enablement at 08:00.

Concept

The main purposes of a fire detection system are to save lives and to minimize damage to buildings and other properties in case of a fire. A fire detection system detects actual fire, risks of fire, and other fire-related events.

Concept

The fire detection panel (FDP) is the control unit of your fire detection system. The panel connects objects in a configuration and allows users to interact with them.