388 Topic(s)
You change the filter conditions to narrow what is displayed in the Alarms pane, Events pane, Alarm View, or Event View.
You sort on alarms and events to get a better overview in the Alarms View or Events View.
You select fields in the Alarm view or Event view to display information regarding alarms and events.
There are several sets of icons for fire graphics. The icons that are used in your fire graphics depend on the selection of icon set in Fire Expert Graphics manager.
The set of Swedish icons is used to display Swedish icons in fire graphics.
The set of Italian icons is used to display Italian icons in fire graphics.
The set of Finnish icons is used to display Finnish icons in fire graphics.
The set of default icons are used in fire graphics when no other set is selected in Fire Expert Graphics manager.
When you force a value, you override all input from the system. For example, if a schedule is set to enable a device at 09:00, but you want to enable it at 08:00, you can force the enablement at 08:00.