418 Topic(s)
Use the Building Operation WorkStation window to log on to WorkStation.
There are several sets of icons for fire graphics. The icons that are used in your fire graphics depend on the selection of icon set in Fire Expert Graphics manager.
The set of Swedish icons is used to display Swedish icons in fire graphics.
The set of Italian icons is used to display Italian icons in fire graphics.
The set of Finnish icons is used to display Finnish icons in fire graphics.
The set of default icons are used in fire graphics when no other set is selected in Fire Expert Graphics manager.
System alarms monitor system entities, such as online status for field servers or field devices. The system alarms are generated by the EcoStruxure Building Operation software. Users cannot create new system alarms. The possible causes of a system alarm are gathered in an enumeration called System alarm ID. When a system alarm is triggered, the cause of the alarm is indicated in the System alarm ID column in the Alarms pane or Alarm View. Some system alarms have additional information in the Alarm text column.
When you force a value, you override all input from the system. For example, if a schedule is set to enable a device at 09:00, but you want to enable it at 08:00, you can force the enablement at 08:00.
The main purposes of a fire detection system are to save lives and to minimize damage to buildings and other properties in case of a fire. A fire detection system detects actual fire, risks of fire, and other fire-related events.