1210 Topic(s)
You start Software Administrator to be able to configure the port settings of the Enterprise Server or Enterprise Central.
You generate an archive by selecting either a CSV or XML format. You can store the archive in Enterprise Server, Enterprise Central, or define a different location.
You use an extended trend log to store records from a trend log. An extended trend log can be connected to a trend log or connected in a series to another extended trend log. Only one extended trend log can be connected to a trend log​ or another extended trend log.
Ensuring the EcoStruxure Building Management integration is installed securely is key to the overall security envelope of the building. The following integration security configurations need to be considered to ensure the overall security meets “best practice” standards.
Use the Options dialog box to manage some local user settings.
Use the Building Operation WorkStation window to log on to WorkStation.
You use theDisplay Names and IP Addresses of Servers drop-down list box to add, edit and delete the display names of the server addresses. You also use it to export, import and delete lists of the display names and IP addresses of servers.
You configure the Archive settings and schedule on the Enterprise Server or Enterprise Central to automate the archiving process.
You edit a backup rule on an EcoStruxure BMS server to change the type of data that you want to back up. You can also set up this backup rule to follow a shadow schedule that references a lead schedule managed on another EcoStruxure BMS server.