earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Registration Portal
Functionalities: Registration
10/30/2025

System Registration

arrow1_rotationOnline Registration arrow1_rotationOffline Registration

As the owner, you register your EcoStruxure BMS to ensure that you are informed in the unlikely event of any critical cybersecurity vulnerabilities that have been discovered in the version you are running, and your system integrator for some reason is unavailable. The information we collect makes potential onboarding to other digital services from Schneider Electric quicker and easier. The information will also help Schneider Electric make more informed decisions in future product development.

You register your EcoStruxure BMS online or offline through EcoStruxure Building Operation WorkStation. If you register online, the registration information you provide is displayed in the WorkStation and WebStation log on page.

For more information, see Online Registration .

For more information, see Offline Registration .

You can verify and edit your registration details any time when needed.

There are several registration options:

  • You can register a stand-alone field server.

  • You can register an Enterprise Server together with connected field servers.

  • You can register an Enterprise Central server together with connected Enterprise Servers and field servers.

Regardless of your system complexity, you register only the server from the top level of your hierarchy. Lower tier servers inherit registration information. The system will use the existing registration whenever possible.

Online Registration

You register an EcoStruxure BMS online when the EcoStruxure Building Operation WorkStation is connected to the Internet.

For more information, see Online Registration .

Offline Registration

You register an EcoStruxure BMS offline when the system is not connected to the Internet. If there is no Internet connection, the system prompts you to offline registration.

For more information, see Offline Registration .

  • WorkStation Overview
  • Online Registration
  • Offline Registration