earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, Esmi Sense FDP
Functionalities: Security
12/2/2024

Generate Certificate Dialog Box

Use the Generate Certificate dialog box to generate a self-signed certificate.

 
action_zoom_plus_stroke Generate certificate dialog box
Figure: Generate certificate dialog box

Table: Generate Certificate Dialog Box

Component

Description

Name

Enter the name of the certificate.

Description

Enter a description of the certificate.

Common name

Enter the certificates common name

Use IP/DNS from communication settings

Select to use the IP address or the DNS address from the communication settings in the EcoStruxure BMS server.

Email address

Enter the email address to the the person responsible for the certificate.

Organizational unit

Enter the organizational unit responsible for the certificate.

Organization

Enter the organization responsible for the certificate.

Locality

Enter the location of the organization or person who is responsible for the certificate.

Country

Select the country.

Valid from

Displays the date from when the certificates is valid. This date is always the current date.

Valid to

Enter the last date the certificate is valid.

  • Certificates
  • Generating a Certificate Using WorkStation