Use the Advanced tab to configure the advanced settings of Connect Agent.
|
Component |
Description |
|
Maximum bandwidth |
Select the bandwidth at which the crash information is to be transfered. If '0' is selected, the crash information is transfered at maximum bandwidth. |