earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Security
12/2/2024

Removing a Certificate Using WorkStation

You remove certificates that you do not want to use anymore.

Show More
action_close

The EcoStruxure Building Operation software supports certificates. Certificates are electronic credentials that are used to certify the identities of computers, and other entities on a network.

The EcoStruxure Building Operation software supports both self-signed certificates and certificates issued by a certificate authority. Certificates are included in a backup and restored on the restored EcoStruxure BMS server.

You can add an existing certificate or generate a certificate. You then activate the certificate.

The access to the certificate management in the EcoStruxure Building Operation software can be set so that certificates can only be handled by authorized users.

Default Certificates

The EcoStruxure Building Operation software uses a default certificate that only supports encryption. The default certificate is installed by default on all EcoStruxure BMS servers. When a user logs on to an EcoStruxure BMS server, the user is notified in the Security certificate risk dialog box that the certificate cannot be validated.

The user must click trust to continue to log on to the system. This dialog box cannot be turned off. The warning is displayed each time the user log on.

Self-Signed Certificate

You can activate a self-signed certificate in EcoStruxure BMS servers. The self-signed certificate can be generated in the EcoStruxure Building Operation software or in another tool.

When the EcoStruxure Building Operation software is used to generate self-signed certificates, certificates can be generated for one or many servers at the same time.

When the user logs on to the EcoStruxure BMS server with an activated self-signed certificate the user is notified if the certificate is not valid. In this case the user can choose to always trust the certificate. If trusted, the self-signed certificate's public key is stored in the certificate list in Windows. The next time the user logs on to the EcoStruxure BMS server, Windows recognizes the certificate and the user can log on without trusting the certificate again.

CA Certificates

The EcoStruxure Building Operation software supports CA certificates, certificates issued by a certificate authority. The supported file format is PEM. Each certificate can include up to three separate files. CA certificate can be installed on a server using both WorkStation and Device Administrator.

For more information, see WorkStation Server CA Certificate Workflow .

Certificates and Licensing

Certificates generated using Workstation cannot be used for licensing in field servers since these certificates do not provide a root certificate or other trust chain for validation. If you use WorkStation certificates, we recommend that you generate new ones for your field servers from Device Administrator when you use licensing in field servers.

For more information, see Certificates Managed using Device Administrator .

Certificates Managed by WorkStation

Certificates are used to increase the security of the communication between EBO servers and clients like WorkStation and WebStation.

For more information, see Certificates Managed Using WorkStation .

Certificates Managed Using Device Administrator

Certificates are used to increase the security of the communication between Device Administrator and field server.

For more information, see Certificates Managed using Device Administrator .

Public Key Infrastructure in EcoStruxure Building Operation

Public Key Infrastructure (PKI) involves managing digital certificates, public and private keys, and other security elements across multiple servers.

For more information, see Public Key Infrastructure in EcoStruxure Building Operation .

To remove a certificate using WorkStation
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.

  2. Click the Control Panel tab.

  3. Under Security and Communication , click Security Settings .

  4. Click Certificates .

  5. Expand Certificate settings .

  6. In the server list, select the servers.

  7. Click Manage Certificates .

  8. In the Manage Certificates dialog box, select the certificate you want to remove.

  9. Click the Remove certificate button

     
    action_zoom_plus_stroke
    .

  10. Click Close .

  • Certificates
  • Control Panel Tab
  • Manage Certificates Dialog Box
  • Adding a Certificate using WorkStation
  • Generating a Certificate Using WorkStation