You can configure the security for WebStation using WorkStation.
In WorkStation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.
Click the Control Panel tab.
Click Security Settings .
Configure the security settings.
Property |
Description |
Enable external websites to be embedded into WebStation |
Select if you want external content to be embedded in WebStation. Enabling external websites to be embedded into WebStation lowers the security significantly. Do not enable external websites to be embedded into WebStation if you do not understand the security implications. For more information, see HTML Utilities . |
Lists external websites that are allowed to be embedded into WebStation |
Type a list of websites that are allowed to be embedded into WebStation. The list is a white list of allowed external websites. Enabling external websites to be embedded into WebStation lowers the security significantly. Do not enable external websites to be embedded into WebStation if you do not understand the security implications. For more information, see HTML Utilities . |
Enable WebStation to be embedded into another site |
Select if you want WebStation to be embedded in another web site. For more information, see Security Configuration in WebStation . |
Website to allow access to WebStation when embedded |
Type a list of websites that are allowed to access WebStation when WebStation is embedded in the website. |
Enable WebStation to use unsafe string evaluated JavaScript methods |
Select if you have graphics written in older versions of EBO that cannot be displayed in 3.0 or later. For more information, see Cannot Open Graphics in WebStation . |
Enable HSTS pre-load list |
HSTS is a preload list supported by Google. It requires a valid certificate on the server. Refer to Google HSTS documentation for more information. |
HSTS pre-load list max-age |
HSTS is a preload list supported by Google. It requires a valid certificate on the server. Refer to Google HSTS documentation for more information. |
Click the Save button