earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Enterprise Central, Enterprise Server, Esmi Sense FDP
Functionalities: Alarms
12/2/2024

System Alarm ID E-L

Listed below are the System Alarms with IDs that begin with the letters E-L.

Table: System Alarms E

System Alarm ID

Description

Email service configuration error

No email server is specified.

Email service failed to connect to SMTP server

The email service failed to connect to the SMTP server.

Email service failed to login to SMTP server

The email service failed to log on to the SMTP server.

Email service failed to send message

The email service failed to send the message.

Email service no recipient email address

There was no recipient to send the email to.

Email service no sender and recipient email address

There was no sender email specified and no recipient to send the email to.

Email service no sender email address

There was no sender email specified.

Error in log definition

Xenta trend log configuration error.

Error in retrieving Xenta device Trend Log data

Xenta trend log retrieving error.

Error - Upgrade using DFU mode

File system is corrupt. Upgrade using DFU mode.

Table: System Alarms F

System Alarm ID

Description

Failed to create object

The attempt to create an object failed.

Failed to initialize references

An object has a reference or binding to a property or another object that cannot be found.

Failure backing up server database

A backup operation failed. If the information is available, the server path and technical reason for the failure is supplied in the alarm information.

Failure restoring server database

A restore operation failed. If the information is available, the alarm also contains the EcoStruxure BMS configuration path for the server that ran the restore.

Failure retrieving backup set from remote server

The Enterprise Server failed to retrieve a newly generated backup set from an Automation server. The name of the Automation server is supplied. If the information is available, the file name of the backup set is also supplied.

File I/O error

Failed to write to file.

Table: System Alarms I

System Alarm ID

Description

Invalid archive path

The archive path is not valid.

Invalid archiving format

The archiving format is not supported.

Invalid device address

The device address is not valid.

Invalid device identifier

The identifier on the specified device is invalid.

Invalid license server configuration

Two or more Enterprise Servers get their licenses from the same license server. This is not the recommended setup.

IO driver unexpectedly timed out

The IO driver timed out unexpectedly.

IO error when generating archive

There is a detected error during the archive generation.

IO error when writing to archive temporary

There is a detected error when the archive is saved to a predefined directory.

IO error, cannot write to archive directory!

There is a detected error when the archive is saved to a predefined directory.

IO error, cannot write to archive directory! Retrying in 5 minutes

There is a detected error when the archive is saved to a predefined directory. The system will restart the archive process in 5 minutes.

IO error, not enough space left in the archive directory

The destination directory does not have enough storage space for the archive.

IO error, not enough space left in the archive directory! Retrying in 5 minutes!

The destination directory does not have enough storage space for the archive. The system will restart the archive process in 5 minutes.

IP connection offline

Modbus TCP connection timeout.

Table: System Alarms L

System Alarm ID

Description

License violation

The amount of required licenses is greater than the amount of existing licenses on the License Server.

Local administrator account has empty or default password

Local administrator account has empty or default password.

Log full

The Xenta trend log is full.

Log stopped because it is full

The Xenta trend log stopped because it is full.

Log variable error

A Xenta trend log variable is missing or invalid.

Logging started

The Xenta trend log started logging.

Logging stopped

The Xenta trend log stopped logging.

  • System Alarm ID List
  • System Alarms
  • System Alarm ID A-D
  • System Alarm ID M-NW8 R
  • System Alarm ID P-S
  • System Alarm ID T-X