Listed below are the System Alarms with IDs that begin with the letters E-L.
|
System Alarm ID |
Description |
|
Email service configuration error |
No email server is specified. |
|
Email service failed to connect to SMTP server |
The email service failed to connect to the SMTP server. |
|
Email service failed to login to SMTP server |
The email service failed to log on to the SMTP server. |
|
Email service failed to send message |
The email service failed to send the message. |
|
Email service no recipient email address |
There was no recipient to send the email to. |
|
Email service no sender and recipient email address |
There was no sender email specified and no recipient to send the email to. |
|
Email service no sender email address |
There was no sender email specified. |
|
Error in log definition |
Xenta trend log configuration error. |
|
Error in retrieving Xenta device Trend Log data |
Xenta trend log retrieving error. |
|
Error - Upgrade using DFU mode |
File system is corrupt. Upgrade using DFU mode. |
|
System Alarm ID |
Description |
|
Failed to create object |
The attempt to create an object failed. |
|
Failed to initialize references |
An object has a reference or binding to a property or another object that cannot be found. |
|
Failure backing up server database |
A backup operation failed. If the information is available, the server path and technical reason for the failure is supplied in the alarm information. |
|
Failure restoring server database |
A restore operation failed. If the information is available, the alarm also contains the EcoStruxure BMS configuration path for the server that ran the restore. |
|
Failure retrieving backup set from remote server |
The Enterprise Server failed to retrieve a newly generated backup set from an Automation server. The name of the Automation server is supplied. If the information is available, the file name of the backup set is also supplied. |
|
File I/O error |
Failed to write to file. |
|
System Alarm ID |
Description |
|
Invalid archive path |
The archive path is not valid. |
|
Invalid archiving format |
The archiving format is not supported. |
|
Invalid device address |
The device address is not valid. |
|
Invalid device identifier |
The identifier on the specified device is invalid. |
|
IO driver unexpectedly timed out |
The IO driver timed out unexpectedly. |
|
IO error when generating archive |
There is a detected error during the archive generation. |
|
IO error when writing to archive temporary |
There is a detected error when the archive is saved to a predefined directory. |
|
IO error, cannot write to archive directory! |
There is a detected error when the archive is saved to a predefined directory. |
|
IO error, cannot write to archive directory! Retrying in 5 minutes |
There is a detected error when the archive is saved to a predefined directory. The system will restart the archive process in 5 minutes. |
|
IO error, not enough space left in the archive directory |
The destination directory does not have enough storage space for the archive. |
|
IO error, not enough space left in the archive directory! Retrying in 5 minutes! |
The destination directory does not have enough storage space for the archive. The system will restart the archive process in 5 minutes. |
|
IP connection offline |
Modbus TCP connection timeout. |
|
System Alarm ID |
Description |
|
License violation |
The amount of required licenses is greater than the amount of existing licenses on the License Server. |
|
Local administrator account has empty or default password |
Local administrator account has empty or default password. |
|
Log full |
The Xenta trend log is full. |
|
Log stopped because it is full |
The Xenta trend log stopped because it is full. |
|
Log variable error |
A Xenta trend log variable is missing or invalid. |
|
Logging started |
The Xenta trend log started logging. |
|
Logging stopped |
The Xenta trend log stopped logging. |