earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, Esmi Sense FDP
Functionalities: Alarms
12/3/2024

Create Object Wizard – Configure Notification Report Template Page

Use the Configure Notification Report Page to configure the properties of the notification report template.

 
action_zoom_plus_stroke Configure Notification Report Template page
Figure: Configure Notification Report Template page

Table: Configure Notification Report Template Page

Property

Description

 
action_zoom_plus_stroke

Add  

Click to add a report data type to the notification report template.

 
action_zoom_plus_stroke

Edit  

Click to edit the properties of the selected report data type.

 
action_zoom_plus_stroke

Remove  

Click to remove the selected report data type.

Report text

Enter text to include in the notification report template.

Quick filter

Enter a word to filter on. For more information, see Quick Filter ..

Substitution codes list

Add the substitution codes you want to use in the notification or notification report.

For more information, see Properties and Watch View Properties Substitution Codes .

For more information, see Trend Log Records Substitution Codes .

Timout(s)

Enter the number of seconds the notification attempts to fetch values from the EcoStruxure Building Operation database before canceling.

First day of week

Select the day to be set as the first day of week.

Time zone

Select the time zone for the notification reports.

  • Notification Reports
  • Notification Report Template View
  • Quick Filter
  • Properties and Watch View Properties Substitution Codes
  • Trend Log Records Substitution Codes