earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Alarms
12/2/2024

Notification Report Template View

Use the Notification Report Template view to view and edit the properties of the notification report template.

 
action_zoom_plus_stroke Notification Report Template view
Figure: Notification Report Template view

Table: Notification Report Template View

Number

Description

 
action_zoom_plus_stroke

Report data

Use the Report data to add, edit, or remove data types in the notification report template.

 
action_zoom_plus_stroke

Quick filter

Use the Quick filter to enter a word to filter on. For more information, see Quick Filter .

 
action_zoom_plus_stroke

Substitution codes list

Use the substitution codes list to drag the substitution codes you want to use to generate the notification or notification report text to the text box.

For more information, see Properties and Watch View Properties Substitution Codes .

For more information, see Trend Log Records Substitution Codes .

 
action_zoom_plus_stroke

Report text

Use the Report text to edit the contents and formatting of the notification report text. For more information, see Notification Reports .

 
action_zoom_plus_stroke

First day of week

Use the first day of week function to select the day to be set as the first day of week.

 
action_zoom_plus_stroke

Time zone type

Use the time zone type function to select a type of time zone.

 
action_zoom_plus_stroke

Time zone

Use the time zone function to select the time zone for the notification reports.

  • Notification Reports
  • Create Object Wizard – Configure Notification Report Template Page
  • Notification Report Template Properties - Basic Tab
  • Quick Filter
  • Properties and Watch View Properties Substitution Codes
  • Trend Log Records Substitution Codes