earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: WorkStation
Functionalities: Basic Functionality, Engineering
12/2/2024

Timed Force Multistate Object

arrow1_rotationState Configuration

The Timed Force Multistate object has a single multistate input that can be bound to another object to receive a value. The input's value is passed directly to a single multistate output, which can be bound to an object that is to be controlled. With a Timed Force Multistate object, you can select and then force the display of a text string associated with one of the states created in the object. An active timed force can be changed or cancelled as needed.

As with other Timed Force objects, the end time of the force can be configured as either a time duration or an end date and time.

State Configuration

The state configuration of a Timed Force Multistate object allows specific multistate values to be associated with text strings. The result is that for a given state, the value displayed to the user is the text string associated with the particular numeric multistate value.

For more information, see Timed Force Multistate Object State Configuration .

  • Timed Force Objects
  • Timed Force Multistate Object State Configuration
  • Timed Force Multistate Object Properties – Basic Tab
  • Timed Force Multistate Object Properties – Parameters Tab
  • Configuring a Timed Force Object for Force Until
  • Configuring a Timed Force Object for Force Duration