earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Enterprise Server, Esmi Sense FDP
Functionalities: Alarms
12/3/2024

Adding an Audio File for a Custom Audible Alarm Alert

You add an audio file that you want to use to configure a custom audio alert for an alarm.

Show More
action_close

A custom audible alarm alert is an audio file that is played when an alarm is triggered.

When several alarms with configured audible alerts are triggered, only the audible alert of the alarm with the highest priority is played. If several alarms with the same priority are triggered, only the audible alert of the latest triggered alarm is played.

To make it easier to find alarms with configured audible alerts in the Alarms pane or an Alarm View, you can combine audible and flashing alerts. You can disable the audible alert of an alarm. The alert is disabled until the alarm is triggered again.

You can configure alarm filters and alarm decoration rules to include custom audible alarm alerts.

Custom Audible Alarm Alert Workflow

To configure a custom audible alert for an alarm, you add the audio file to the EcoStruxure BMS server and then connect the alarm to the audio file.

For more information, see Custom Audible Alarm Alert Workflow .

Audio Files

The following audio file formats are supported:

  • m4a

  • mp3

  • mp4

  • wav

  • wma

You save the audio files you want to use for custom audible alarm alerts in the System folder of the EcoStruxure BMS server where the audio file is to be played. You have to log on to the server where the audio files are saved to hear the custom audible alarm alerts.

To hear custom audible alerts for all alarms in a multi-server system when logged on to an Enterprise Central, add the audio files to the System folder of the Enterprise Central.

To hear custom audible alerts for all alarms in a multi-server system when logged on to an Enterprise Server, add the audio files to the System folder of the Enterprise Server.

To hear custom audible alarm alerts when logged on to a field server, add the audio files to the System folder of that field server.

To add an audio file for a custom audible alarm alert
  1. In WorkStation, expand the EcoStruxure BMS server where the audio file is to be played.

  2. On the EcoStruxure BMS server where the audio file is to be played, select the Audio folder in the System folder.

  3. On the File menu, point to New and then click Audio file .

  4. In the Create Object wizard, in the list, select the audio file format of the audio file you want to add.

  5. In the Name box, type a name for the audio file.

  6. In the Description box, type a description for the audio file.

  7. Click Next .

  8. In the Audio file box, enter the path of the audio file.

  9. Click Create .

The audio file can now be connected to the audible alert of an alarm.

  • Custom Audible Alarm Alerts
  • Create Alarm Wizard – Presentation Page
  • Configuring a Custom Audible Alarm Alert