earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Alarms
12/3/2024

Custom Audible Alarm Alert Workflow

A custom audible alarm alert is an audio file that is played when an alarm is triggered.

 
action_zoom_plus_stroke Custom audible alarm alert flowchart
Figure: Custom audible alarm alert flowchart
Add an Audio File for a Custom Audible Alarm Alert

Add the custom audio file to the EcoStruxure BMS server where you want to hear the custom audible alarm alert.

For more information, see Adding an Audio File for a Custom Audible Alarm Alert .

Configure a Custom Audible Alarm Alert

Configure the alarm to play the custom audio file when the alarm is triggered or reset.

For more information, see Configuring a Custom Audible Alarm Alert .

  • Custom Audible Alarm Alerts
  • Alarm Functions
  • Adding an Audio File for a Custom Audible Alarm Alert
  • Configuring a Custom Audible Alarm Alert