earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Trends
12/2/2024

Manual Trend Log Properties – Meter Info Tab

Use the Meter Info tab to configure the meter function of the trend log.

 
action_zoom_plus_stroke Meter Info tab
Figure: Meter Info tab

Table: Meter Info Tab

Property

Description

Is meter log

Displays True if the trend log meter function is active.

For more information, see Meter Function .

Meter change time

Displays the time when the meter was changed.

Meter change user

Displays the name of the user account that changed the meter.

End time

Displays the time when the old meter was replaced.

End value

Displays the value the old meter had when it was replaced.

Start time

Displays the time when the new meter was installed.

Start value

Displays the value of the new meter when it was installed.

Meter constant

Displays the constant of the new meter. If the meter counts in kilo (10 3 ), the constant is 1000.

Min value

Displays the first value of the new meter after roll-over.

Max value

Displays the last value of the new meter before roll-over.

  • Manual Trend Logs
  • Meter Function
  • Configure Dialog Box – Configuration Tab
  • Manual Trend Log Properties – Basic Tab
  • References Tab