earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Alarms, Engineering
12/3/2024

Configure Alarm Filters on Enterprise Central Workflow

Alarm filters are used to set up the conditions for the alarms you want to be displayed in an Alarms pane or an Alarm View. You also use alarm filters to determine the conditions that have to be met before a sum alarm is triggered, an email notification is sent, a write to file notification is written, or an alarm is automatically assigned to a user.

 
action_zoom_plus_stroke Custom audible alarm alert flowchart
Figure: Custom audible alarm alert flowchart
Synchrone Alarm Control Panels

Synchronize Alarm Control Panels to configure a lead-shadow relationship between Enterprise Central and the Enterprise Server on which the alarms reside.

For more information, see Synchronizing Alarm Control Panels .

Create a Category

On Enterprise Central, create the alarm Category 2 for the the Enterprise Server or field server alarms you want to display on Enterprise Central.

For more information, see Creating a Category .

Create an Alarm Decoration Rule

On Enterprise Central, create an alarm decoration rule to override one or several properties of aggregated alarms when the conditions of the alarm decoration rule are met. For this chosen condition, configure Category 2.

For more information, see Creating an Alarm Decoration Rule .

Create a Filtered Alarm View

On Enterprise Central, create a filtered Alarm View that only displays the Category 2 alarms.

For more information, see Creating a Filtered Alarm View .

  • Alarm Filters
  • Alarm Categories
  • Alarm Decoration
  • Synchronizing Alarm Control Panels
  • Configuring the Category of an Alarm
  • Creating an Alarm Decoration Rule
  • Creating a Filtered Alarm View
  • Enterprise Central